{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Control Expert15,SP1 returns Integrity Check error.
Attempts to run Control Expert 15, SP1 after installing returns the following Integrity Check error:
c c



This can occur if there is more than one' **IntegrityCheckHash.dll' file located in the folder named 'C:\Program Files (x86)\Common Files\Schneider Electric Shared\SRCSDK'.
ccc cz



To resolve the issue, either rename the file or delete the file.
zxc

Schneider Electric Egypt and North East Africa