{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum number of ASi modules supported by the M580 PLC platform ?
Issue:
Max number of ASi modules supported by the M580


Product Line:
EcoStruxure Control Expert, BMXEIA0100


Resolution:
The following maximum number of AS-i modules on a local rack containing one of the following CPUs is allowed.
  • BMEP581020:   2 modules
  • BMEP582020:   4 modules
  • BMEP582040:   4 modules
  • BMEP583020:   6 modules
  • BMEP583040:   6 modules
  • BMEP584020:   8 modules
  • BMEP584040:   8 modules
  • BMEP585040:   8 modules
  • BMEP586040:   8 modules

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: