{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
EcoStruxure Automation Expert [21.1]:How to resolve the issue "Deploy Plugin AvevaServerPlugin not installed" ?

This knowledge base helps the user to resolve the "Deploy Plugin AvevaServerPlugin not installed" issue that comes under the Deploy and diagnostic tab when the AVEVA_SERVER device is being used in the project?
The error message shows as below highlighted in Yellow color
issue

The issue is happening as the mandatory plugin required for AVEVA_SERVER device is not installed in the machine.

The AvevaServerPlugin can be installed  either by reinstall/repair the Ecostruxure Automation Expert

The user needs to select the "AutoBuild AVEVA InTouch OMI" for any of the highlighted selections and complete the installation procedure.
NOTE: The Default selection is "This Feature will not be available".Hence plugin is not getting installed by default.
solution

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: