{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to configure the Momentary ON function on the web visualization when using HMISTW6?

Some web visualization applications designed with Machine Expert include the buttons with the Momentary ON function (the buttons that keep the variable value on TRUE as long the operator presses the buttons). The default configuration of the visualization Manager does not allow to use the Momentary ON function on the HMISTW6.
The goal of this article is to inform about the right configuration of the visualization Manager in order to use the Momentary ON function on the HMISTW6.

This article is applicable to the following products:
HMISTW6 range.

This topic is related to the Machine Expert using the web visualization function.

From the settings of visualization Manager, we need to activate the function called “Activate multitouch handling” in order to use the Momentary ON function on the HMISTW6 (see attached file)
Visualization Manager settings to use the Momentary ON function

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: