{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to configure AFDD ( Arc fault Detection Device) in Ecostruxure power design-Ecodial?

Article available in these languages: Spanish

In Ecodial, Below are the steps to configure AFDD.
Step-1
  • Create the network
  • Ensure that the AFD is getting used in 50HZ & Single phase network and up to 25A (NL) & 40A (FR) only for final loads


Step-2
  • Select the Circuit breaker in the Feeder
  • Enable the AFD


Step-3
  • Run the calculation for the automatic selection of the AFD



Step 4
  • For manual selection of AFD, Click on it
  • Select AFD selection tab for more options

Step 5
  • Check the specification and validate as per requirement

Step 6
  • Run the calculation



Step 7
  • The Feeder is successfully incorporated with AFDD.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.