{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to set up Somove to connect to a ATV340 Drive using CANopen.

Issue:

How can you connect Somove using the CANopen connection option?

Product Line:

ATV61, ATV71, ATV320 and ATV340 only

Environment:

All

Cause:

Connection using CANopen

Resolution:

You will need to use a CANopen USB-CAN Dongle ( Port 1 only is supported) if you have a dual port.

This connection option is only supported with the ATV61, ATV71, ATV320 and ATV340 Drives only. You can not use this option on the ATV630 or ATV930 drives.

See the attached document on setting up Somove to use CANopen.

Schneider Electric Egypt and North East Africa

Attachment(s)
SoMove CANopen connection instructions.pdf [674.32 KB]