{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the difference between TeSys Giga advanced and standard type contactors ?

The advanced type has 3 coil variants to cover 24V-500V control voltage, PLC control input, lower coil consumption, cable memory kit, feasibility to fix Remote wear Diagnosis (RWD) module.
Whereas the standard version comes with two coil variants to cover 48-250V control voltage, normal coil consumption and with direct coil control by A1/A2.
Both advanced and standard versions have self-diagnosis LED on the front of the contactor to indicate the main contact life, over and under voltage indication, internal fault indication etc..

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: