{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can the customer run his ATV212 drive at 80 hz max?

Issue:

Customer wants to run his ATV212 drive at 80 hz max.

Product Line:

ATV212

Environment:

Analog input scaling

Cause:

Using 0-10v input

Resolution:

Go to FH- set to 80, UL- set to 80.

Also need to adjust the scaling parameters:

For VIA - go to F201-0, F202-0, F203=100, F204-set to 80

For VIB - go to F210-0, F211-0, F212=100, F213-set to 80

Schneider Electric Egypt and North East Africa