{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which Microsoft Windows operating system is supported by EcoStruxure Control Expert 15 and 15SP1?
Issue:
Microsoft Windows operating systems supported by EcoStruxure Control Expert 15 and 15SP1


Product Line:
EcoStruxure Control Expert


Resolution:
EcoStruxure Control Expert V15 and V15SP1 is supported on the following Microsoft Windows operating systems
-Windows 10 64bits( version 1809 minimum is mandatory), Note: Windows 10 32 bits not supported
-Windows 10 Enterprise 2019 LTSC (version 1804)
-Windows Server 2019 (Standard version is recommended)

Schneider Electric Egypt and North East Africa