{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you use an external 24VDC to power up an ATV340 drive?

Issue:

Customer wants to use an external 24VDC supply to power up an ATV340 drive

Product Line:

ATV340

Environment:

All

Cause:

Power drive up without line voltage for programming

Resolution:

Yes you can use an external 24VDC to power the ATV340 drive for programming. Bring the external supply to 24V (+) and 0V (-) terminals. Note: The external +24 Vdc controller supply must meet the requirements of IEC 61131-2 (PELV standard power supply unit).

Schneider Electric Egypt and North East Africa