Issue:
IDLF faults on a ATV680 enclosed product
Product Line:
ATV680
Environment:
IDLF faults
Cause:
n/a
Resolution:
When the device is in IDLE mode and you send a run command, but the device does not start to charge the bus within the adjusted energy saving timeout [idLt] (Factory settings: 5s // 8s for ATVx80 and ATVxB0), then the device will trip with IDLF.
Probable cause: The mains voltage is missing and the device cannot charge the DC Bus.
Remedies :Check mains voltage and ensure its availability. Check the DC bus voltage
Released for:Schneider Electric Egypt and North East Africa