{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the TA1 -TA4 parameters in the ATV61/ATV71 drives?

Issue:
TA1 -TA4 parameters in the ATV61/ATV71 drives.

Product Line:

ATV61/ATV71 drives

Environment:

TA1- TA4 parameters

Cause:

n/a

Resolution:

TA1 (Rounding of the start of the ACC ramp) -Factory default is 10%

TA2 (Rounding of the end of the ACC ramp)-Factory default is 10%

TA3 (Rounding of the start of the DEC ramp)-Factory default is 10%

TA4 (Rounding of the end of the DEC ramp)-Factory default is 10%

Schneider Electric Egypt and North East Africa