{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to solve Integrity Check error reported with EcoStruxure Control Expert V15.0 Classic
1. Issue
Integrity Check error is reported after having uninstall and reinstall EcoStruxure Control Expert V15.0 Classic.
Two cases can happen:
Case 1 : You already previously installed hot fixes for Control Expert V15.0  (e.g. ControlExpert_CEV150_HF_New_Ethernet_Module_Limitation).
Then you uninstalled and reinstalled Control Expert V15.0.

Case 2: You already have previous versions of Control Expert installed and at first Control Expert V15.0 installation the Integrity Check error is reported.


2. Resolution
Case 1 : To solve the issue it is mandatory to reinstall all hot fixes previously installed.
This issue will be definitively corrected with EcoStruxure Control Expert V15.0 SP1.

Case 2: You need to remove the folder named SSTA from the path  "C:\Program Files (x86)\Common Files\Schneider Electric Shared\".
Then do a repair of your Control Expert V15.0.

Schneider Electric Egypt and North East Africa