{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I perform an auto diagnostics test on an ATV61/71?
Issue:
Needs to run an auto diagnostics test on an ATV61 to verify the state of the internal components.

Product line:
Altivar 61/71

Environment:
All models, all serial numbers

Cause:
Getting short circuit faults, needs to run a diagnostics test form the drive.

Resolution:

From Drive Menu, go to Menu 1.10 DIAGNOSTICS:

image.png

Then Go to option "Test Procedures" and press Enter on the desired test, a caution message will appear. To start the tests, press and hold down (2 s) the ENT key.

image.png


The result for each IGBT is displayed on 2 lines:
- The first line shows whether or not it has short-circuited
- The second line shows whether or not it is open

Notes:
[TEST THYRISTORS] is only accessible for ATV61...M3 => 18.5 kW, ATV61...N4 drives => 18.5 kW, and all ratings of ATV61...Y drives.
Test results for Thyristor 4...12 and IGBT 1B...6B are only accessible for ATV61EC90N4 to M14N4 and ATV61EM15Y to M24Y

Schneider Electric Egypt and North East Africa