{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the coil control voltages available for TeSys Giga ?

Article available in these languages: Dutch

TeSys Giga contactor is available in advanced version and standard version. Both advanced and standard version have different type of control voltages.
Advanced versionStandard version
24…48V AC/DC*
48…130V AC/DC
200…500V AC/DC
48…130V AC/DC
100…250V AC/DC
*not available for 630-800A

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.