{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why is there no output voltage, when the ATV71 drive is running?

Issue:

No output voltage from the ATV71 drive

Product Line:

ATV71/ATV621

Environment:

output voltage

Cause:

n/a

Resolution:

Power down and perform static checks on the outputs to the +/- bus ( PA/+ to PC/-).

Power up the drive and recheck all the motor parameters, including the Motor control Type parameter.

Then could go to 1.10 menu and run the transistor tests.

If all these test pass, then make sure the Motor Control Type is set to V/F 2 pts ( 1.4 menu)

and then go to 1.8 menu: set OPL to no. Run the drive at 20, 40 and 60 hz and measure

all the outputs to see if they are all balanced. If they are balanced, then appears the drive

is ok. Would suggest to disconnect the motor and megger it out with 1000v megger.

Schneider Electric Egypt and North East Africa