{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to set Timeout Value for Modbus TCP/IP driver in Vijeo Designer 6.2?

You can use the driver property @prop:0 to set timeout value for Modbus TCP/IP driver in Vijeo Designer 6.2. Use this parameter to set a timeout value between 2 to 15 seconds for this driver. The timeout value determines the amount of time the driver takes to attempt a reconnect after a detected connection loss. Write an integer value from 2 to 15 to @prop:0 to set the timeout value.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: