{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can you setup the ATV320 drive so that its in ATV32 identifier mode to allow ATV32 CANopen EDS files?

Article available in these languages: Spanish

Issue:

ATV320 drive so that its in ATV32 identifier mode?

Product Line:

ATV320 series

Environment:

All

Cause:

Wants to use existing CANopen EDS files from the ATV32 on the ATV320 replacement drives.

Resolution:

When using ATV32 EDS file under CANopen in Advantys:

  • If the drive ATV320 has version less than version V2.9IE34à the drive used a mechanism with hidden parameter ( AP12), so you can used ATV320 as ATV32 ( Like with Advantys with ATV32 EDS).
  • If the drive ATV320 has version equal or greater then version V2.9IE34 --> AP12 is replaced by NTID parameter.

NTID Fieldbus Identifier selection CANopen address is 5F in hex. Its a R/WS address. WS means you can write to the parameter if the drive is stopped.

NTID= 1 Drive will be identified as a ATV32 drive.

NTID= 0 Drive will be identified as a ATV320 drive.

Schneider Electric Egypt and North East Africa