{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

EcoStruxure Power Operation 2021: VCRUNTIME140.dll Error during installation while configuring 'Configure PostgreSQL' step

Article available in these languages: Spanish

Issue
During installation of Power Operation 2021 below popup with error ‘’ observed during 'Configure PostgreSQL' step.
The code execution cannot proceed because VCRUNTIME140.dll was not found.

Some times above popup is not visible, but below error is present inside install log file.
RunExecutableWithReturn received an error from command E:\setup\SetupSupport\PostgreSQL\postgresql-13.3-2-windows-x64.exe --mode unattended --unattendedmodeui none --prefix "C:\Program Files\postgreSQL" --datadir "C:\ProgramData\Schneider Electric\Power Operation\v2021\database" --superaccount postgres --superpassword ****** --debugtrace "C:\Program Files (x86)\Schneider Electric\Power Operation\v2021\SetupLogs\postgresql.log" --disable-components pgAdmin Error running C:\Users\EMSCEMENT\AppData\Local\Temp\postgresql_installer_0a8b5943a0\getlocales.exe : child killed: unknown signal

Environment

Power SCADA Operation (PSO) 2020
EcoStruxure Power Operation (EPO) 2021


Cause
Corrupt Microsoft Visual C++ 2015 Redistributable which is already installed (from some 3rd party apps) in the machine in which required DLL file is missing in the windows directory is causing this issue.


Resolution
Uninstall the existing 'Microsoft Visual C++ 2015 Redistributable' from control panel-


Then install them from the PO ISO (or Microsoft site) and installed
Now 'Retry Failed step' which will resume the configuration and installation will be successful.

Schneider Electric Egypt and North East Africa

Explore more
Range:
EcoStruxure™ Power Operation
Explore more
Range:
EcoStruxure™ Power Operation
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.