Search FAQs
What is the best practice to add custom measurement in PME?
Issue
How to add custom measurement with metadata
Product Line
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Environment
Manual Data Editor
Cause
The best practice to add a custom measurement before adding is by using the “Manual Data Editor”.
The main reasons are:
Resolution
Manual Data Editor is found in the Management Console (Tools tab -> System -> Manual Data Editor).
You can use Manual Data Editor to create new, custom measurements in PME. These measurements are available anywhere in the software.
To create a new measurement:
How to add custom measurement with metadata
Product Line
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Environment
Manual Data Editor
Cause
The best practice to add a custom measurement before adding is by using the “Manual Data Editor”.
The main reasons are:
- Manual Data Editor adheres to naming convention rules in PME,
- Special Characters are largely restricted
- The most common predicates can be set up in the interface
- Cumulative, Unit, Aggregation
Resolution
Manual Data Editor is found in the Management Console (Tools tab -> System -> Manual Data Editor).
You can use Manual Data Editor to create new, custom measurements in PME. These measurements are available anywhere in the software.
To create a new measurement:
- In Manual Data Editor, click Load New Data to open the Load Data dialog box.
NOTE: Load Data opens automatically when you start Manual Data Editor.
- In Load Data, click Create new Measurement to open the Create new Measurement dialog box.
NOTE: Check the list of available measurements to see if one exists for your application before creating a new measurement.
- In Create new Measurement, enter the relevant information for the new measurement.
- Click Create to add the new measurement to the system.
- (Optional) Repeat steps 2-4 to add additional measurements.
- Close Manual Data Editor.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: