{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Coupling switch requirement in DRS architectures
DRS architectures that require Main Ring / Sub Ring redundant connections (coupling switches) must be of the same type of switch.

The example shows a C7 master and a C8 slave configuration for DRS function, with the main ring copper ports and RIO subring ports copper. In this case, both switches must be of same type, either Connexium or Modicon.  They cannot be mixed types, that is, one Connexium and the other Modicon.

Other switches in the ring can be mixed but the coupled pair (Master/Slave) MUST be the same brand type as shown below.

DRS Modicon-Connexium example


For further information, reference the Modicon M580 System Planning Guide for Complex Topologies, part number NHA58892.

Main Ring / Sub-Ring Redundant Connections - General Information
Use 2 DRSs (one installed with a master predefined configuration and the other installed with a corresponding slave predefined configuration) to provide a redundant connection between the main ring and the sub-ring. The master DRS passes data between the main ring and the sub-ring. If the master DRS becomes inoperable, the slave DRS takes control and passes data between the main ring and the sub-ring.


Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: