{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Will upgrading the firmware on an APC PDU cause loss of power to the outlets?
Issue:
Will the firmware upgrade process on my APC PDU cause the unit to stop supplying power to its outlets?

Product Line:
APC Rack PDU - AP7xxxB, AP8xxx and APDU9xxx


Cause:
As long as the PDU is operating normally and there are no active alarms, a firmware upgrade of the management interface will not power on/off any attached loads.
The network management card will reboot during the process, but this will not affect the attached load.

Schneider Electric Egypt and North East Africa