{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
The 170ADM39030 Datasheet incorrectly shows the input and output voltages
The 170ADM39030 datasheet posted on se.com prior to March 2022 incorrectly showed the Discrete Input voltage as 20…115 VAC.
It should be, 24 VDC, (11…30 VDC).

The datasheet also incorrectly showed the Discrete Output voltage as only 20…115 VDC.
It should be, 20…115 VDC, 24…230 VAC.


This identifies where in the datasheet the corrections will be applied.

170ADM39030 datasheet corrections
Note that the User Guide shows the correct Discrete Input and Discrete Output voltages.


Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: