Search FAQs
How do I perform the surge arrester SPD arrester wiring in EVlink Pro AC ?
With EVlink Pro AC, the SPD is installed in the switchboard of the customer's installation.
With Evlink Pro AC Metal the SPD can be installed in the case of the charging station. For more information see:
Electrical diagram EVlink Pro AC Metal_GEX2008001.
With Evlink Pro AC Metal the SPD can be installed in the case of the charging station. For more information see:
Electrical diagram EVlink Pro AC Metal_GEX2008001.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: