{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a direct replacement for the XBTGH2460 HMI?

Issue:

Is there a direct replacement for the XBTGH2460 HMI?

Product Line:

XBTGH

Resolution:

Unfortunately, per our Marketing team, there will not be a replacement for the XBTGH in the future due to low sales volume.

If you are looking for an HMI with membrane keys and a touchscreen, you could look into the HMIGK line of HMIs. The HMIGK's does not have a built in estop.

One could also look into the HMIGTO line of HMIs for a full touchscreen panel without membrane keys.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: