{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I increase the Torque on the motor, on a ATV930 drive?

Issue:

How can I increase the Torque on the motor, on a ATV930 drive?

Product Line:

ATV930

Environment:

Increase torque

Cause:

n/a

Resolution:

Go to Complete Settings

Select Motor Parameters Recheck all the motor parameters to make sure they match the motor.

Check the rating of the drive to see if you can set Dual rating to Heavy duty?

Motor Control Type- suggest to set to SVC V

Motor Data- Motor Param Choice set to Mot CoSinus, set Motor 1 Cosius Phi to ,81 ( or the

PF on the motor nameplate)

Motor Control-IR Compensation – increase as needed, to provide more torque. Slip

compensation- decrease setting, as needed.

Go back to Motor Data and select 2nd function key (Tune) and auto tune ONLY if the motor

is cold.

Schneider Electric Egypt and North East Africa