{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which Miniature Circuit Breaker protection devices need to be installed with EVlink Pro AC ?
The charging station shall be protected by the following devices (provide this set of protections for each socket):
Circuit Breaker 40A Curve C for each socket 7.4 kW (1P+N) or 22 kW (3P+N)
Circuit Breaker 20A Curve C for each socket 11 kW (3P+N)
Consult the Installation Guide (ref: NNZ1940301 or JYT24398) available on se.com.

Schneider Electric Egypt and North East Africa