BMXDAI16142 not found in the selection list for adding modules to the rack.
In order to add a BMXDAI16142 module to the rack in Control Expert, the BMXDAI1614 needs to be selected. The configuration of a BMXDAI16142 is the same as that for a BMXDAI1614
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
EcoStruxure Control Expert (Unity Pro)
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.