{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the Status code STO on Process Drives?
Issue:
STO on AT600 and ATV900 Drives.

Product Line:
Altivar Process Drives

Environment:
All

Cause:
NA

Resolution:
STO is not a fault code.  It is a state of the drive.  It means that Safe Torque Off function is active. The drive is not detecting 24Vdc on the STOA or STOB terminals.
Measure for 24Vdc between +24 to COM to verify the internal power supply. If you don't have 24 Vdc present on the +24 terminal, measure DC voltage between PA+ and PC- to check your DC bus voltage.
Confirm that the factory installed jumper between +24 to STOA & STOB is solidly connected.  The jumper is removed if a safety circuit is installed.  Verify continuity of the safety circuit (if installed).
Make sure the Sink/Source switch is in the Source position.
When the voltage on STOA and STOB is re-established, the drive status will return to RDY if there is not an active run command, or NST if a run command is active.  To clear NST, remove the run command.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.