undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
PDPM288G6H: Install Manual Requires 4-wire Input. Is 3-Wire Acceptable?
Issue:
The installation manual requires a 4-Wire (3 phases + Neutral + PE) for the input and output.  This PDU has a transformer in it.  Can it be installed as a 3-Wire (3 phases + PE) on the input with the transformer creating a Neutral on the output for the load?

Product line:
Modular PDU

Environment:
All models, all serial numbers

Cause:
Customer requested information since 4-wire wasn’t available in the installation location.  The installation manual, one-line diagrams, and the service manual do not provide specification as to why 4-wire is required.
One Line Diagram
Resolution:
No, this PDU requires 4-wire on the input and output.
The input neutral is required since it is the same neutral used for the output.  The Auto Transformer doesn’t have a Star Point to create a the neutral needed by the load.
Neutral Connection PointTransformer Connections

Schneider Electric Egypt and North East Africa

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.