{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I configure the cybersecurity settings of BMENUA0100 OPC UA Server module ?

Issue:
configuring the cybersecurity settings of BMENUA0100 OPC UA Server module


Product Line:
EcoStruxure Control Expert, BMENUA0100


Resolution:
below are the steps to Configure the cybersecurity settings of the OPC UA server module:

1. With the module detached from the rack, use the plastic screwdriver that ships with the module to set the rotary switch to the [Secured] position.
2. Install the module into an Ethernet slot on the local, main Ethernet rack and cycle power.
3. Use your Internet browser to connect your configuration PC to the module, using either the control port or the backplane port, and navigate to the module web pages at the configured IP address.
4. If your Internet browser displays a message indicating a potential security risk, proceed to make the connection by clicking Accept the Risk and Continue (or similar, browser-specific language).
5. In the user login page, enter the default username / password combination.
6. Change and confirm the password. Refer to the User Management topic for password requirements. The module Home page is displayed.
7. Starting from the Home page, navigate to the module web pages and configure its cybersecurity settings.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: