{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Altivar Process (ATV600/ATV900) drives be used at high altitude?

Issue:

Customer wants to use the ATV630 at elevation over the maximum elevation listed in the Manual (1000 meters).

Product Line:

Altivar 600 series (ATV630, ATV650, ATV660, ATV680)

Altivar 900 series (ATV930, ATV950, ATV960, ATV980)

Environment:

Altitude over 1000 meters

Cause:

High elevation jobsite

Resolution:

See the following table for details on derating when used at high elevation.

derating table

Schneider Electric Egypt and North East Africa