{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to upgrade the firmware of a TSXETG3000 module ?
The following steps need to be performed :
  1. Download the Web Designer version of the firmware version needed for the TSXETG3000.
  2. Unzip the iso file and store the 'Firmware Upgrade'.folder in your PC.
  3. Open a DOS command window as an administrator and run the 'Upgrade.bat' file from the 'Firrmware Upgrade' folder
  4. Wait until the ETG3000 stopped flashing after receiving the "  'Download Firmware Complete' and 'Type E to Exit'  " message in the DOS command window.
  5. Wait until the RUN Light is on solid.
  6. Power cycle the ETG3000.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: