{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible replace a PRM without Control Expert?

Yes , it is possible.


In Control Expert application, in the PRM general settings:
Option "Create an entry for this device name in DHCP server" and "backup the PRM configuration in FDR server on download" must be checked and well configured.

Then the following steps must be performed to replace properly the PRM :

1- Remove the PRM module to be replaced

2-Take a new PRM:

  1. Set its lower rotary switch in 'E' position ( Configuration file deletion) in order to clear existing configuration file
  2. Power up the new PRM and wait for the PRM boot completion, then power off the PRM module
  3. Check the positions of the rotary switch of the old PRM module and set the rotary switch of the new PRM identically.
  4. Power up the PRM on the same location as the old one

The new PRM will boot and take its configuration file from the FDR server.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: