Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Why is the "œ" character not displayed correctly during EcoStruxure Operator Terminal Expert runtime?

Issue: 
Character "œ" appears incorrectly during Runtime

Product Line:
EcoStruxure Operator Terminal Expert, Harmony HMI,

Resolution:
The language fonts on EcoStruxure Operator Terminal Expert are regulated by ISO standards.
 
The French_Gothic font set uses the character code [ISO IEC8859-1]. The "œ" character can not be displayed because it is a character that does not exist in the [ISO IEC 8859-1] character code.
 
Instead, use the Romanian_Gothic font set. This uses the character code [ISO IEC8859-16] which includes the "œ" character.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: