{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: eConversion Live from the Lab 2: Mains Outage
eConversion is a patented high-efficiency mode for Schneider Electric Galaxy V Series (VS, VM, VL, VX) UPS that combines the best efficiency (up to 99%) with maximum load protection (IEC62040-3 class 1, VFI1.1.1 – equivalent to Double Conversion).
eConversion typically provides a 3x reduction of the UPS electricity consumption. This live video from the lab shows the system behavior in case of a mains outage.
Discover more via eConversion Savings Calculator .

Schneider Electric Egypt and North East Africa