{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: eConversion Live from the Lab 3: Power Factor Correction
eConversion is a patented high-efficiency mode for Schneider Electric Galaxy V Series (VS, VM, VL, VX) UPS that combines the best efficiency (up to 99%) with maximum load protection (IEC62040-3 class 1, VFI1.1.1 – equivalent to Double Conversion). eConversion typically provides a 3x reduction of the UPS electricity consumption.
This live video from the lab shows how eConversion performs input power factor correction.
Discover more via eConversion Savings Calculator.

Schneider Electric Egypt and North East Africa