{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PM2020/PME2021 web report represents incorrect values when the report "Measurements Selector" changes between from one mode to another mode (Smart Mode/Detailed Mode)
Issue
In PM2020/PME2021 web report represents incorrect values when the report Measurements Selector changed from one mode to another mode (Smart Mode/Detailed Mode). Different values are shown for same measurement selected in different mode as shown below

IM1
IM2

Product Line
PME 2020
PME 2021

Environment
PME 2020 with or without CU
PME 2021 with or without CU

Cause
In PME 2020 and PME 2021 when a report measurement selector is configured with detailed mode and then if the measurement selection is switched/changed to smart mode then the report gives incorrect data. This is because the measurement selected in detailed mode is not cleared during the change of measurement selection mode. Please refer the below illustration

Detailed mode selection

First in detailed mode the selected measurement is “Real Energy into The Load”
DM1
DM2

Please refer the attached report “Energy Usage Report” for the result.
Smart Mode:
Then the report measurement selection is changed to smart mode “Real Energy” but the already selected measurement “Real Energy into The Load” is not shown in measurements.
SM1
SM2

Please refer the attached report “Energy Usage Report (1)” for the result, it is a summation of both the measurement.


Resolution

Whenever the report measurement input mode is changed make sure that the measurement selected in previous mode is cleared first before changing the mode.

This workaround will fix the issue.

NOTE:
This issue is fixed in PME next release PME2022.

Schneider Electric Egypt and North East Africa

Attachment(s)
Energy Usage Report (1).xls [195 KB]
Energy Usage Report.xls [197.5 KB]
Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: