{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is the communication time out managed when using an Ethernet option card with the ATV600 series drive?
Issue:
The RPI setting does not appear to impact the Communication timeout as described in the option card manual.

Product Line:
Altivar 600 series drives: ATV630, ATV650, ATV660, ATV680 when using Ethernet option cards VW3A3720 or VW3A3721

Cause:
Documentation needs updated

Resolution:
The communication timeout related to the Ethernet option card is an internal parameter TOUT (register 64211, units are 0.1 seconds).
This parameter can be accessed using SoMove by adjusting the Holdup Time under the Modbus TCP settings in the option card tab.  The time set applies to both Modbus TCP and Ethernet IP communications.

Attach Video here:

Schneider Electric Egypt and North East Africa

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: