Search FAQs
Can OFS Server communicate to an M340 via the USB port?
Issue:
OFS server communication to M340 USB port
Product Line:
OFS Server, M340
Resolution:
Yes, OFS Server can communicate to an M340 PLC via the USB port. To configure the OFS server to communicate to the M340 via USB, launch the OFS configuration tool. Then create an alias by selecting "File" then "New Device Alias". Next click on the ellipsis for Device address 1 to add the USB driver. Select M340 for the Device type and add the symbol table file. Save the configuration
Select the USB driver as shown and select ok.
OFS server communication to M340 USB port
Product Line:
OFS Server, M340
Resolution:
Yes, OFS Server can communicate to an M340 PLC via the USB port. To configure the OFS server to communicate to the M340 via USB, launch the OFS configuration tool. Then create an alias by selecting "File" then "New Device Alias". Next click on the ellipsis for Device address 1 to add the USB driver. Select M340 for the Device type and add the symbol table file. Save the configuration
Select the USB driver as shown and select ok.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Product:
Explore more
Product: