{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How must I configure OPC UA communications when an IPSEC tunnel is configured?
In the case where secured OPC UA client connect to the BMENUA server and IPSEC tunnels are activated to the clients, by default the OPC UA connections will pass inside the tunnel. For the best performances, we recommend configuring the product in order to pass these OPC UA connections outside the tunnel. This can be done as following:
  • ADD a new FORWARDING rule,
  • Select OPC UA protocol,
  • Inbound interface CONTROL PORT or BOTH,
  • uncheck IPSEC in use in order to force OPC UA traffic to pass outside the IPSEC tunnel

Product Line

BMENUA0100 version 2.01

Environment

Windows, EADM

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: