{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How I set up ATS22 for Ramp Stop?
Issue:
Decelerate the motor with ATS22 Softstarter instead of Freewheel.

Product Line:
ATS22

Environment:
All

Cause:
Need ramp stop

Resolution:
Do not jumper LI1 to LI2. Wire LI1 to CL1, use run contact between CL1 and LI2, and program SEt - dEC = ramp down time.
The factory default setting for the dEC parameter is 'free'.

Schneider Electric Egypt and North East Africa