{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an MDLF or MultiDrive link error on the ATV930 Drives?

Issue:

MultiDrive link error on the ATV930 Drives?

Product Line:

ATV930

Environment:

All

Cause:

MultiDrive link error can be triggered due to communication interruption between Server and Client drive. It can also be triggered if Multi Drive link function has detected an inconsistency in the system configuration.

Resolution:

Check the communication network.

Check the configuration of the multi-drive link function.

Check the firmware and make sure it is consistent on both drives.

Schneider Electric Egypt and North East Africa