{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I get the standby CPU to run automatically after program transfer?

Issue

Automatically run standby CPU after transfer of program

Product Line

M580

Environment

EcoStruxure Control Expert

Resolution

To have the standby CPU run automatically after a transfer you need to set the CMD_RUN_AFTER_TRANSFER bit before you transfer to the standby controller. You can set this in an animation table or you could hard code this bit to always be true in your first section of logic.

img1

Schneider Electric Egypt and North East Africa