{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the Modbus Plus MBX Drivers work on Windows 11?

Issue

Windows 11 support

Product Line

TSXCUSBMBP

Environment

Modbus Plus

Resolution

The latest MBX drivers (v9.0) will work on Windows 10 and 11. The part number for the drivers only is SWMXDS001. If you were to purchase an adapter with part number TSXCUSBMBP you would also get a copy of the drivers.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: