{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
EcoStruxure Power Operation (EPO) 2021: Graphics editor crashes after duplicating a new component

Issue
When grouping several objects together as a component; after a few copies and pastes of the new component in the Graphics Editor, the application crashes with the following error message:

Graphics Editor – Unexpected Error
Object reference not set to an instance of an object

Error Message

The Graphics Editor application doesn't open again unless deleting the TGML file from the TGML folder.

Product Line
EcoStruxure Power Operation 2021 CU2/ CU3

Environment
Graphics Editor

Cause
When you copy and paste a new component, a new property called InstanceId is created under custom properties. InstanceID is unique but causes the application failure.

Resolution
The workaround is to delete the Instanceld property. Please right-click and delete the InstanceId line under Custom.

InstanceID Location

Note: The problem will be addressed in future updates.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: