Search FAQs
What IP Services are enabled on my SCADAPack x70 RTU
Is there an easy way to see what IP services my SCADAPack x70 device is configured for?
Open the saved RemoteConnect project or else read a configuration from a x70 device using RemoteConnect. In the RemoteConnect Configuration DTM, select SCADAPack in the on the Configuration tab.
The IP services that are possible for configuration are listed. For those ports with green arrows to the right of them, these can be configured and the green arrow will bring the user to the configuration page. Ports items such as Telnet or FTP cannot be changed, yet they can be enabled or disabled.
![IP Services x70](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000D2Lj4QAF&oid=00DA0000000abSmMAI)
Further information about IP services can be found in the RemoteConnect help manuals installed with RemoteConnect.
Open the saved RemoteConnect project or else read a configuration from a x70 device using RemoteConnect. In the RemoteConnect Configuration DTM, select SCADAPack in the on the Configuration tab.
The IP services that are possible for configuration are listed. For those ports with green arrows to the right of them, these can be configured and the green arrow will bring the user to the configuration page. Ports items such as Telnet or FTP cannot be changed, yet they can be enabled or disabled.
Further information about IP services can be found in the RemoteConnect help manuals installed with RemoteConnect.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: