{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
P3 IEC61850 LN value update failure
Issue
After IEC61850 configuration in P3 relay, customer found that some LN was not updating the actual value.
1
_____________________________________________________________
Product Line

Easergy P3 relay
_____________________________________________________________

Environment
All firmware version
_____________________________________________________________
Root Cause
Customer didn’t enable the “Event ON/OFF” which is related to the LN, so the change in value is not updated to LN.
2

3 4
_____________________________________________________________
Solution
1- If our customer want to use some LNs in P3 relay, especially for GGIO LNs, customer should enable separate “Event ON/OFF” function as shown below.
ItemLN(example)Event ON/OFF
Digital input115
Logical output126
Protection137
Virtual input148


2- It will be updated to the manual in future release.
_____________________________________________________________





=====End of document=====

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.