{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Unable to access NMC3 via HTTPS using Chrome - ERR_CERT_INVALID
Problem:
Users are unable to access an NMC3 with a self-signed certificate via HTTPS using recent versions of the Google Chrome browser

Environment:
UPS Network Management Card 3 - AP9640/41/43
Devices that use an embedded NMC3, including but not limited to PDU (2022+ model AP8xxx, APDU9xxx), ATS (AP44xxA), and Smart-UPS/Symmetra UPS systems

Cause:
A recent Chrome update is blocking the self-signed certificate ECC certificate that is used by default on an NMC3.

Resolution:
This will be addressed in a future version of firmware, and this article will be updated when a fix version is available.

Please note that this issue is fixed from firmware rev. 2.4, so updating firmware should be fist step in the troubleshooting process.

Secondary work-arounds are:
  • Use a different browser
  • Use an older version of Chrome
  • Delete the ECC self-signed certificate on the NMC and generate an RSA cert. The commands can be performed via the CLI:
    • apc>ssl key -d
    • apc>ssl key -rsa [1024|2048|4096]
  • Use the CLI Security Wizard and a 3rd party certificate authority to create a signed certificate

Schneider Electric Egypt and North East Africa