Search FAQs
How do I setup the BMENOC0321 module to send an email based on predefined events or conditions via explicit exchange messaging?
Issue:
Setting up the BMENOC0321 module to send an email based on predefined events or conditions via explicit exchange messaging??
Product Line:
Ecostruxure Control Expert, BMENOC0321
Resolution:
Based on predefined events or conditions, it is possible to send email messages using the explicit exchange message block SEND_EMAIL. First ensure that the email service of the NOC module is enabled via the DTM configuration
![email](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DAWA6QAP&oid=00DA0000000abSmMAI)
Under the "EMAIL" section, specify the SMTP server IP address and port number. This is where you would also enter the header information such as the subject, sender and recipient email address. If authentication is necessary, enable and enter the credentials if not, disable it.
![email2](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DAWA7QAP&oid=00DA0000000abSmMAI)
sample of the address structure for the SEND_EMAIL function block via the ADDM block
![email3](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DAWCHQA5&oid=00DA0000000abSmMAI)
Note: To test the email functionality of the module, you can use a free SMTP server that runs locally on your PC such as Argosoft.
Setting up the BMENOC0321 module to send an email based on predefined events or conditions via explicit exchange messaging??
Product Line:
Ecostruxure Control Expert, BMENOC0321
Resolution:
Based on predefined events or conditions, it is possible to send email messages using the explicit exchange message block SEND_EMAIL. First ensure that the email service of the NOC module is enabled via the DTM configuration
Under the "EMAIL" section, specify the SMTP server IP address and port number. This is where you would also enter the header information such as the subject, sender and recipient email address. If authentication is necessary, enable and enter the credentials if not, disable it.
sample of the address structure for the SEND_EMAIL function block via the ADDM block
Note: To test the email functionality of the module, you can use a free SMTP server that runs locally on your PC such as Argosoft.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Product:
Explore more
Product: